web counter

What is a Ground Fault Circuit Interrupter?

Published: 22 April 2021 | Last Updated: 27 March 20255859
A ground fault circuit interrupter(GFCI) is an electrical device installed to protect against severe electric shocks. It can also reduce electrocutions, minimize electrical burns and shock injuries, and detect ground faults, and interrupts the flow of electric current.
How to replace a GFCI outlet with a new outlet. How to perform handyman work.

How To Replace A GFCI Outlet / Step By Step

A GFCI is not be used to replace a fuse and does not protect against circuit overloads, short circuits, or shocks. Its working voltage is 264VAC-102VAC, working temperature is 35Deg~66Deg. America has very strict GFCI certifications which mainly include UL and ETL certification, if you do UL certification, all tests of products are carried out in UL laboratory in the United States; if ETL certification is done, tests can be carried out in China.


Catalog:

I Classification
II Characteristic
III Working Principle
IV Application
V Main brand


I Classification


According to different wiring methods, GFCI can be divided into:

1.Receptacle-type ground-fault circuit-interrupter

The protector uses a socket to output and connects with the plug of the load equipment.

2.Portable ground-fault circuit-interrupter Portable ground-fault circuit-interrupter

The protector uses a plug to connect to the socket of the power supply circuit, and the position of the protector relative to the power supply circuit is not fixed. The parts of the protector (including the protector shell and the output socket) can be easily moved. According to the distance between the protector shell and the plug, it can be divided into:

a.Plug-in ground-fault circuit-interrupter 

The protector shell is glued to the plug as a whole, and the shell and the output socket are connected by cables or wires.

6159252dd42a2834b88dc49a5bb5c9ea15cebf7c[1].jpg

Figure 1:  Plug-in ground-fault circuit-interrupter 

b. In-line type ground-fault circuit-interrupter

Cables and wires with plugs are drawn from the protector shell, and the plugs are connected with the sockets of the power supply circuit. The protector shell and the output socket shell can be made into a whole or can be connected by cables or wires.

f286d7b60a67198997258824bb84a4a.png

Figure 2: In-line type ground-fault circuit-interrupter


II Characteristic


Because GFCI detects ground faults, it can also prevent some electrical fires. In a household wiring system, on a power outlet, under normal circumstances, the current of the hot wire and the neutral wire should be equal. GFCI monitors the current difference. If the difference is greater than 6 mA (according to the UL943 standard, when the leakage current is 6mA, the disconnection time is 25 milliseconds), it can cut off the power at 0.025s (disconnection time when the leakage current is 4-6mA in the case of 500-ohm impedance according to the UL943 standard) to ensure personal safety. The GFCI interrupts power faster than a blink of an eye to preventing lethal power. You may receive a painful shock, but you will not be electrocuted or receive severe shock injuries.

All GFCIs should be tested every time when they are used to ensure that they can work properly and to protect you from fatal shocks. GFCI should be inspected after installation to ensure they can work and properly protect the circuit. To test the GFCI socket, first, plug the nightlight or lamp into the power socket, then the light should be on at that time. When pressing the "TEST" button, the "RESET" button of the GFCI should pop up and the light will go out. If you press the "reset" button, it pops up, but the nightlight is not off. In this situation, the GFCI has been improperly wired. Contact an electrician to correct the wiring error. If you press the "reset" button, it does not pop up, which shows that the GFCI is defective and should be replaced.


III Working Principle


GFCI uses the circuit to detect the opening or closing of the circuit, and the Reset Button (or indicator light) displays the current state of the circuit so that the user can know whether the circuit is currently in a normal working state or a faulty state. In order to improve the safety of use, an auxiliary switch is set to control the power supply of the circuit board to prevent the circuit board from being damaged due to current overload. It is designed to have the function of automatically disconnecting the circuit to avoid electric shock caused by foreign matter in the load, that is when the live wire of the working circuit is grounded through the foreign matter. This kind of function is for some customers who are at risk of electric shock, when a strong current flows through their bodies, the power supply will be automatically removed.

GFCI checks the balance of the current flowing through the live wire and the neutral wire. If the neutral wire current suddenly becomes much smaller than the live wire current, an electric shock may have occurred. A part of the current flows back to the ground wire through a loop outside the neutral wire. If the current of this part is between 4.2mA and 5.8mA, or greater, GFCI will send out a pulse that cuts the power of the load circuit through a mechanical structure. GFCI limits the time that the electric shock current flows through the body of the shocked person instead of the size of the current. This time is calculated based on physiological data to avoid damage to the health of ordinary people. GFCI has a simple appearance and inherits the original functions of GFCI products. The operation of Bridge Contacts strengthens the ability to solve faults caused by the reverse connection of the power input line and the load output line, and prevents the loss caused by the initial wiring errors of the installer, thus further improving the function of the leakage protector. 

What to do if the GFCI trips:

In some cases, GFCI’s will trip but this does not mean that there is something wrong with the installation. One of the reasons that the GFCI is tripping is that it is installed in circuits longer than 100 feet. When there are many splices, fluorescent lighting fixtures, or permanently installed electric motors in the circuit, there will be another problem because this can cause the GFCI to trip. If the GFCI is installed in circuits longer than 100 feet, this could be one of the reasons your interrupter is tripping. Another issue can occur when the circuit has many splices, fluorescent lighting fixtures, or permanently installed electric motors as this can cause the GFCI to trip. When using the protection with freezers, garage door controls before installing a GFCI, the power may be cut. Be aware that during the installation, the lines and/or loads should be properly landed to ensure that the device will work properly, if not, the GFCI will not reset, so you should make sure the connections are right.  The GFCI is not the same as the ACFI. The AFCI is used to address fire hazards, while GFCI is installed to prevent shock hazards. 


IV Application


GFCI can be widely used in high-pressure electric washing machines, electric lawnmowers, electric water pumps, large electric bathtubs, electric harvesters, electric water mills, electric cutting machines, hand-held power tools, etc.


V  Main brands


In the US market, plug-type GFCI is commonly seen, and its brands have LEVITON, TOWER, ELEGRP, DEFOND, NANDAO, etc. In the domestic market, leakage protection heads and leakage protection sockets are commonly seen. Suzhou Lumeisi Electric Co., Ltd. has 15 years of production experience in GFCI. It independently researches and develops, and produces GFCI, GAB, Jiaanbao, and leakage protection walls. Its products include five series: leakage protection series, leakage overcurrent protection, intelligent protection, current limiting protection, and Camry.

American Leviton (LEVITON), founded in 1906, headquartered in New York, is a global leader in the manufacture of electrical accessories, lighting control, energy management, and structured wiring products. Leviton has 35 factories worldwide, mainly in the United States, Canada, Mexico, and China. All factories have passed ISO9001/2001 certification and have highly automated production lines; provide a complete set of high-quality products and services, including design, modeling, production, and logistics. 

American TOWER is affiliated with the American TMC (Tower Manufacturing Corporation). TMC, founded in 1957 and headquartered in Rhode Island, is a professional manufacturer of switch products. The products involve GFCI, ALCI, LCDI, and other professional leakage protection products. All are applicable in different industries and products and have obtained UL certification. It has wholly-owned subsidiary factories in the United States and Shenzhen, China, as well as a branch in Hong Kong. The company has a complete R&D, design, production, sales, and after-sales service team.

ELEGRP is the only private company to obtain UL certification in the field of portable leakage protectors. It was established in Shanghai in 2000 and has four branches. At the end of 2010, it relocated to Suzhou Industrial Park. Its main markets distribute in the United States and Canada. It has more than ten years of experience in the North American leakage protector market. The products involve professional leakage protector products such as GFCI, LCDI, PRCD, etc. Relying on its own strong R&D capabilities, it has solved technical difficulties and avoided the United States patents, independently designed and developed products, and obtained several Chinese patents and US patents. The company also produces other series products of wiring devices, such as switches, plugs, sockets, etc., all of which have obtained UL and CUL certification.

DEFOND and NANDAO are mainly Hong Kong and domestic companies. Among them, DEFOND has also begun to involve other industries, including automotive electronic parts.


Reference

  1. Guardian GFCI (n.d.). GFCI Defined. https://www.guardiangfci.com/knowledge/gfci-defined

  2. Electrical Technology (2024). GFCI (Ground Fault Circuit Interrupter) - How Does it Work?  https://www.electricaltechnology.org/2015/02/gfci-ground-fault-circuit-interrupter-types-working.html

  3. Harvard Environmental Health & Safety (2014). Ground Fault Circuit Interrupter (GFCI) Fact Sheet.  https://www.ehs.harvard.edu/sites/default/files/ground_fault_circuit_interrupter_gfci_fact_sheet.pdf

  4. Electrical Safety Foundation International (n.d.). GFCIs. https://www.esfi.org/resource/gfci-safety-101-0 0

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.Are ground fault circuit interrupters dangerous?

Current values above 6 milliamperes are considered dangerous! Ground fault circuit interrupters must sense and operate when the ground current exceeds 6 milliamperes. Figure 1b – A small amount of current is induced in the coil because of the unbalance of current in the conductors UL Standard No. 943 covers ground fault circuit interrupters.

2.What is the principle of ground fault circuit?

Figures 1a and 1b show the basic principle of how a ground fault circuit interrupter operates. No current is induced in the coil because both wires are carrying the same current. The ground fault circuit interrupter does not trip the circuit off. A small amount of current is induced in the coil because of the unbalance of current in the conductors.

3.When does the GFCI interrupt the electrical current?

When the amount going differs from the amount returning by approximately 5 milliamperes, the GFCI interrupts the current. The GFCI is rated to trip quickly enough to prevent an electrical incident.

4.What is a GFCI outlet and where is one needed?

GFCI protection is required for 125-volt to 250-volt receptacles supplied by single-phase branch circuits rated 150 volts or less to the ground. GFCI receptacles are required in bathrooms, garages, crawl spaces, basements, laundry rooms and areas where a water source is present.

5.Can I put a GFCI anywhere in a circuit?

You can replace almost any electrical outlet with a GFCI outlet. Correctly wired GFCIs will also protect other outlets on the same circuit. While it's common to find GFCI outlets in bathrooms and kitchens, there are GFCI outlet requirements.
Related Articles

  • What Size Wire for a 60 Amp Breaker? The Complete NEC Guide
    What Size Wire for a 60 Amp Breaker? The Complete NEC Guide
    UTMEL22 May 20266975

    Selecting the right wire size for a 60-amp breaker requires evaluating conductor materials, insulation, and distance. While 6 AWG copper THHN or 4 AWG aluminum in conduit is standard, NM-B Romex limits 6 AWG to 55 amps, requiring 4 AWG copper. Additionally, installers must account for continuous load limits, ground wire sizing, and voltage drop over long runs.

    Read More
  • What is Surge?
    What is Surge?
    UTMEL09 February 20227205

    Hello everyone, I am Rose. Today I will introduce surge to you. Surge is an overvoltage that occurs suddenly and surpasses the typical operating voltage. A surge is a brief wave of current, voltage, or power in a circuit, in general.

    Read More
  • Surge Protection Devices (SPD): The Complete 2025 Guide
    Surge Protection Devices (SPD): The Complete 2025 Guide
    UTMEL25 December 202528950

    A surge protection device (SPD), also called a surge protector, is an electronic device that provides safety protection for various electronic equipment, instruments, and communication lines. When a spike current or voltage is suddenly generated in the electrical circuit or communication circuit due to external interference, the surge protection device can conduct and shunt in a very short time, so as to prevent the surge from damaging other equipment in the circuit.

    Read More
  • What is a Ground Fault Circuit Interrupter?
    What is a Ground Fault Circuit Interrupter?
    UTMEL27 March 20255859

    A ground fault circuit interrupter(GFCI) is an electrical device installed to protect against severe electric shocks. It can also reduce electrocutions, minimize electrical burns and shock injuries, and detect ground faults, and interrupts the flow of electric current.

    Read More
  • What is Vacuum Circuit Breaker?
    What is Vacuum Circuit Breaker?
    UTMEL12 October 202110406

    Hello, I am Rose. Welcome to the new post today. The name "vacuum circuit breaker" comes from the fact that both the arc extinguishing medium and the insulating medium of the contact gap after arc extinguishing are high vacuum; it has the advantages of compact size, light weight, frequent operation, and no arc extinguishing maintenance. This article introduces basis knowledge about vacuum circuit breaker.

    Read More

Subscribe to Utmel !

Featured Parts More